Microphone model on ReSpeaker

We are trying to use “ReSpeaker 6-Mic Circular Array kit for Raspberry Pi” and “ReSpeaker Core v2.0” for an application.



Our application requires each MEMS microphone on board removed and re-connected with shielded cable,

and we would like to know the model of microphones in case they were broken during refactoring process.



Unfortunately, we have not found any information of the model in wiki pages so far.

If it is possible, please let us know that.

Hi palette1972,



ReSpeakers are using Analog MEMS Microphone AOS3729A-T42-NXC and you can find the datasheet here : <LINK_TEXT text="https://datasheet.lcsc.com/szlcsc/18121 … 38759.pdf ">https://datasheet.lcsc.com/szlcsc/1812121637_SANICO-AOS3729A-T42-NXC_C338759.pdf </LINK_TEXT>

Hi,

I’m using ReSpeaker 4-Mic Array for Raspberry Pi and I’m wondering if this micArray is using the same microphone as the one you mentioned!
Or is there any where I can find information about more details about the microphone on ReSpeaker Array?

Thank you in advance!

Best,
Nana

(Update)
I’ve found microphone information from the schematic of ReSpeaker 4-Mic Array for Raspberry Pi!
The microphone is SPU0414HR5H-SB instead, with datasheet here: Access to this page has been denied.

ReSpeaker 4-Mic Array for Raspberry Pi Resources

Source: ReSpeaker 4-Mic Array for Raspberry Pi | Seeed Studio Wiki

Hi,

I’m kinda confused.

According to the schematic from

I found the mic type as SPU0414HR5H-SB on the last page.

However, I checked the MEM mics on my ReSpeaker Mic Array and found that they look much more similar to the mic type mentioned here:

which should be MSM321A3729H9CP.

Therefore, I’m guessing that the PDF file from the website is incorrect.

Best,
Nana Chang

I believe the schematic version is the original one, @Baozhu can you please confirm! Thanks.

@jiachenglu Please help check it.

Hi @Nana_Chang
I have checked the microphone material list, the 4-Mic Array model is MSM321A3729H9BP.
Here is the datasheet. https://files.seeedstudio.com/products/103030216/MSM321A3729H9BP.pdf

@jiachenglu
Hi
I have a question regarding the Respeaker 4-Mic Array.

(https://www.seeedstudio.com/ReSpeaker-4-Mic-Array-for-Raspberry-Pi.html)

Looking at the product images on the above site, it seems that there are two types of microphones mounted on the Respeaker 4-Mic Array.

The gold-colored microphones appear to be SPU0414HR5H-SB(Knowles). However, I am unsure about the model number of the black-colored microphones.

Is the model number of the black microphones MSM321A3729H9BP?

Also, would it be possible to share the source of this information (e.g., material list)?

BR,