Just wondering if this using the same microcontroller?
http://leaflabs.com/devices/maple/
I feel yes. The suffices are different though. One in the maple is rb and the one in the DSO is VCT.
Yes, they are basically the same. The letters indicate the package type (and number of pins) and flash memory size for instance:
R = 64 pins, V = 100 pins
B = 128 KB flash, C = 256 KB
T = LQFP package
I wonder if the quad can be programmed using their ide? I think the bootloader they are using is different.