MicroBit Grove Inventor Kit - Gesture movements

Hi, can you please upload a video demonstrating what the gestures look like for the different options:



I can use left, right and wave, although if I start the wave too slow, the gesture picks up left or right.



Forward, Backward (do these mean proximity to the sensor?)

Up and Down (are these on the same plane as left and right?)

Clockwise and anti-clockwise (is the gesture sensor sensitive enough to not see these as left/right or wave?)



Thank you in advance for your help.

Hi there,



Forward, Backward (do these mean proximity to the sensor?)

Yes



Up and Down (are these on the same plane as left and right?)

Yes, if put the sensor on top, Grove wire at light side, you side will be up and the other side will be down.



Clockwise and anti-clockwise (is the gesture sensor sensitive enough to not see these as left/right or wave?)

If you move the finger a little bit faster, it will detect Clockwise and anti-clockwise effectively.



Here is a demo.

[youtube]https://youtu.be/VONQQrAC-MI[/youtube]



thanks.

Bill