I have today recieved the DSO Nano. I have bought a 2GB micro SD card and installed it. I have inserted the USB cable and I can see a removable drive letter for the SD card. I have formatted it using WIN XP SP3, asking for a regular FAT formatting.
I have also dowloaded the SDFILE %281%29.rar file, and extracted all the FILE000.DAT through FILE039.DAT files onto this Micro SD drive.
But when I try to save or load to/from any of these files, I get the errors:
By FS: File NoPlace
By FL: FILE NoFound
Before the pressing of OK button, I can scroll to select which filename out of the FILE0XX, so the DSO Nano seems to recognize their existance om teh Micro SD card.
Also the USB-connected Laptop can see all the fiels.
What may be wrong? The manual does not reveal an detaild handling information at all…