Meanwell PSU for powering the Odyssey X86

Hi! I’d like to know if, using a Meanwelll RPS-200-12 to power the board through usb-c or jack, could be possible to use the board built-in sata power for a m.2 to pcie x16 extension with a low power gpu? Or do I need to power the pcie directly from the psu?

Thanks a lot!

Hi @wesbluemarine

The maximum output for the Power SATA is 12V@2A, you may want to consider external power source on GPU.