Based on a Matlab TMP102 tutorial I tried to use the lines for a MCP9808 I2C sensor temperature Grove sensor.
What should be the temperature equation as I can not find any information for it (I am using 2019a)?
clear;
aBoard = arduino(‘COM3’, ‘Uno’, ‘Libraries’, ‘I2C’);
addrs = scanI2CBus(aBoard)
tmpGroveSensor = device(aBoard,‘I2CAddress’,‘0x18’)
write(tmpGroveSensor, 0, ‘uint8’);
data = read(tmpGroveSensor, 2, ‘uint8’);
temperature = (double(bitshift(int16(data(1)), 4)) + double(bitshift(int16(data(2)), -4))) * 0.0625
Hi There

the image convey the meaning that ethir you should Convert binary to decimal for Centigrade