Hi, I want to know how much current I can draw from the 5v pin on the seeed studio ESP32C3.
I already checked that the 5v pin is directly connected to the USBc port. However, the conductor track from the USBc port to the 5v pin is only 0.4mm thick.
I want to draw about 2 to 3 amps to power some addressable LEDs. Can the conductor track handle this? I find no information about the 5v pins performance.
Because otherwise I have to use a second USBc port right next to the seeed studio.
LG Simon
No Guts No Glory , so Let us Know…I bet it last for about the time it gets too hot
but you may be surprised
GL
PJ
Under normal circumstances, the XIAO’s operating voltage is 3.3V, if you use 5V power supply, although it is within the safe voltage range, but it will not actually affect the XIAO’s normal supply voltage and maximum output current.