Matter on ESP32C6

Just got my board, confirmed blink sketch works perfectly. But the Arduino IDE examples for Matter (MatterCommissionTest.ino and MatterMinimum.ino) fail on this board because the sketch is too big: Sketch uses 1579565 bytes (120%) of program storage space. Maximum is 1310720 bytes. I’m surprised by this because this device is specifically marketed as supporting Matter. Is there a specific Matter library or other solution?

Hi there,

It does, The issue is between the keyboard and the floor…Half way anyway, You see it only onboards with ESP-IDF for C6 it’s noted in the wiki, However I was able to flash a New XiaoESP32C6 with ESP LaunchPad. You forgot to set some tools menu Items No?, It does require the BIGGEST partition Scheme , the default of course won’t fit, Pick "Hughe APP 3MB_No OTA 1Meg Spiffs "option
Have a Look again…or use the LaunchPad to test it.
HTH
GL :slight_smile: PJ :v:

I flashed this New Xiao unit in less than 30 seconds added it to my devices in milliseconds.

esptool.js
Serial port WebSerial VendorID 0x303a ProductID 0x1001
Connecting....
Detecting chip type... ESP32-C6
Chip is ESP32-C6 (revision 1)
Features: Wi-Fi 6,BT 5,IEEE802.15.4
Crystal is 40MHz
MAC: 54:32:04:11:ee:24
Uploading stub...
Running stub...
Stub running...
Changing baudrate to 921600
Changed
Manufacturer: 0
Device: 00
Detected flash size: undefined
Warning: Image file at 0x0 doesn't look like an image file, so not changing any flash settings.
Compressed 1835488 bytes to 1039071...
Writing at 0x0... (1%)
Writing at 0x214b4... (3%)
Writing at 0x2fdf5... (4%)
Writing at 0x3d66e... (6%)
Writing at 0x4adaa... (7%)
Writing at 0x534c3... (9%)
Writing at 0x58467... (10%)
Writing at 0x5f327... (12%)
Writing at 0x65f72... (14%)
Writing at 0x6c19d... (15%)
Writing at 0x722b2... (17%)
Writing at 0x78b20... (18%)
Writing at 0x80028... (20%)
Writing at 0x85cb1... (21%)
Writing at 0x8c225... (23%)
Writing at 0x94623... (25%)
Writing at 0x9a5b4... (26%)
Writing at 0xa087a... (28%)
Writing at 0xa6cee... (29%)
Writing at 0xad25d... (31%)
Writing at 0xb38eb... (32%)
Writing at 0xba996... (34%)
Writing at 0xc142e... (35%)
Writing at 0xc72bf... (37%)
Writing at 0xcd471... (39%)
Writing at 0xd3128... (40%)
Writing at 0xd8c48... (42%)
Writing at 0xdec56... (43%)
Writing at 0xe4f17... (45%)
Writing at 0xeaf5c... (46%)
Writing at 0xf120d... (48%)
Writing at 0xf73d9... (50%)
Writing at 0xfd5db... (51%)
Writing at 0x10314b... (53%)
Writing at 0x108d80... (54%)
Writing at 0x10f04d... (56%)
Writing at 0x114c56... (57%)
Writing at 0x11aa44... (59%)
Writing at 0x121256... (60%)
Writing at 0x12717d... (62%)
Writing at 0x12f27c... (64%)
Writing at 0x13563e... (65%)
Writing at 0x13b22e... (67%)
Writing at 0x141702... (68%)
Writing at 0x147446... (70%)
Writing at 0x14d32b... (71%)
Writing at 0x153c58... (73%)
Writing at 0x15a0f5... (75%)
Writing at 0x160322... (76%)
Writing at 0x1663d9... (78%)
Writing at 0x16c802... (79%)
Writing at 0x1727cf... (81%)
Writing at 0x178a50... (82%)
Writing at 0x17ecc5... (84%)
Writing at 0x18506a... (85%)
Writing at 0x18af7f... (87%)
Writing at 0x191418... (89%)
Writing at 0x19736d... (90%)
Writing at 0x19d85b... (92%)
Writing at 0x1a3aae... (93%)
Writing at 0x1a9b38... (95%)
Writing at 0x1afdd5... (96%)
Writing at 0x1b5f6e... (98%)
Writing at 0x1bc3ca... (100%)
Wrote 1835488 bytes (1039071 compressed) at 0x0 in 13.609 seconds.
Leaving...

Be sure to press reset for it to discover your new device :v:

Thanks man. Appreciate the heads up on the existence of a wiki.

Curious if you were able to eventually get yours added in milliseconds, too. Flashing with LaunchPad works for me, but after successfully connecting to Google Home the device is seen but shown as disconnected. Trying several times after deleting from Home, re-flashing the ESP32C6 and adding it again as a new device results in the same thing. Following the Espressif LaunchPad video instructions and attempting to connect with and Amazon Echo (4th gen) results in the device never being found. Attempting to connect the device to Home Assistant also results in the device never being found.

Hi there,

Yes, it worked first try? I had to move close to the Echo I have for it to show up and bond. I had to use the mobile app to add it to HA. After it was AOK. :+1:

HTH
GL :slight_smile: PJ :v: