Hello
Can i read a button press on the main power button and use it to perform a certain function?
And can i change the shutdown timeout on the power button from 2 seconds to 10 seconds for example.
Thank you.
Hi, the button can be act as normal button.
please refer to …\Eclipse 2.0.46\LINKIT_ASSIST_SDK\examples\API\Framework_Keypad
But long press to turn off can’t be change, it’s set in the firmware.
Thanks.