Hi,
I am working for a company which one of it’s products is using a M2 light hotspot with the US915 standard. We are currently trying to expand to different countries and this would lead to transferring our product back and fourth between countries.
Is it possible to convert an existing Sensecap M2 light hotspot into another standard? Say for example from US915 into EU868? If the hardware is capable I imagine it would only involve changing the antenna to the appropriate standard and updating the antenna information and location on the helium network.
Or is it that each Sensecap for each standard is only capable of outputting a specific frequency? In that case can it move at least from different standards but same frequency, for example US915 to AU915.
Thank you.