Hello,
I have the similar issue as Rafal. I have the European version of the U-blox Lara R211 and when trying to connect it with RPi 2 model B according to the manual, I only receive the ‘infinite’ waking up.
I successfully managed to connect to the Telekom’s LTE network and to ping google with the help of Windows and the M-Center though, so the LTE device is operational.
My questions might be somewhat dumb, but I just wanna make sure that I am doing everything right:
- In the wiki manual, it is not specifically stated how do you guys connect the LTE module to the RPi. Do you imply connection via USB or UART?
- When I connected to the Telekom’s LTE network via M-Center and Windows, I used the Telekom’s Sim-Card and it had a Pin-Code, which I had to input to the GUI in order to access the network. Could it be the reason why Rpi cannot wake the modem up?
- So, as I mentioned before, I have the RPi 2 Model B V1.1. However, the demo was performed at RPi 3 Model B. Could it be a compatibility issue somehow?
Thanks beforehand for any advice!
Cheers,
Gleb