Hi Felix
Do you go through below 4 steps? I went through the process again. I get the response from board as below. Maybe you can connect the module to windows pc to test the AT command separately to see if it works. Here is the instructions. http://wiki.seeedstudio.com/LTE_Cat_1_Pi_HAT/#faq. thanks.
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------
Software¶
Step 1. Use dtoverlay=pi3-disable-bt to enable Raspberry Pi3 UART0.
sudo nano /boot/config.txt
Then add dtoverlay=pi3-disable-bt to bottom of the config.txt
Step 2. Disable the system serivce to use the UART0.
sudo systemctl disable hciuart
Note
Pi3-disable-bt disables the Bluetooth device and restores UART0/ttyAMA0 to GPIOs 14 and 15. It is also necessary to disable the system service that initialises the modem so it doesn’t use the UART: sudo systemctl disable hciuart.
Step 3. Delete the console=serial0,115200 in cmdline.txt.
sudo nano /boot/cmdline.txt
Then delete console=serial0,115200 from the string.
Step 4. Reboot the Raspberry Pi3
sudo reboot
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------
pi@raspberrypi:~ $ git clone <LINK_TEXT text=“https://github.com/Seeed-Studio/ublox_l … pi_hat.git”>https://github.com/Seeed-Studio/ublox_lara_r2_pi_hat.git</LINK_TEXT>
Cloning into ‘ublox_lara_r2_pi_hat’…
remote: Counting objects: 60, done.
remote: Total 60 (delta 0), reused 0 (delta 0), pack-reused 60
Unpacking objects: 100% (60/60), done.
pi@raspberrypi:~ $ cd ublox_lara_r2_pi_hat
pi@raspberrypi:~/ublox_lara_r2_pi_hat $ sudo python setup.py install
running install
running bdist_egg
running egg_info
creating ublox_lara_r2.egg-info
writing requirements to ublox_lara_r2.egg-info/requires.txt
writing ublox_lara_r2.egg-info/PKG-INFO
writing top-level names to ublox_lara_r2.egg-info/top_level.txt
writing dependency_links to ublox_lara_r2.egg-info/dependency_links.txt
writing manifest file ‘ublox_lara_r2.egg-info/SOURCES.txt’
reading manifest file ‘ublox_lara_r2.egg-info/SOURCES.txt’
writing manifest file ‘ublox_lara_r2.egg-info/SOURCES.txt’
installing library code to build/bdist.linux-armv7l/egg
running install_lib
running build_py
creating build
creating build/lib.linux-armv7l-2.7
creating build/lib.linux-armv7l-2.7/ublox_lara_r2
copying ublox_lara_r2/init.py -> build/lib.linux-armv7l-2.7/ublox_lara_r2
copying ublox_lara_r2/ublox_lara_r2.py -> build/lib.linux-armv7l-2.7/ublox_lara_r2
creating build/bdist.linux-armv7l
creating build/bdist.linux-armv7l/egg
creating build/bdist.linux-armv7l/egg/ublox_lara_r2
copying build/lib.linux-armv7l-2.7/ublox_lara_r2/init.py -> build/bdist.linux-armv7l/egg/ublox_lara_r2
copying build/lib.linux-armv7l-2.7/ublox_lara_r2/ublox_lara_r2.py -> build/bdist.linux-armv7l/egg/ublox_lara_r2
byte-compiling build/bdist.linux-armv7l/egg/ublox_lara_r2/init.py to init.pyc
byte-compiling build/bdist.linux-armv7l/egg/ublox_lara_r2/ublox_lara_r2.py to ublox_lara_r2.pyc
creating build/bdist.linux-armv7l/egg/EGG-INFO
installing scripts to build/bdist.linux-armv7l/egg/EGG-INFO/scripts
running install_scripts
running build_scripts
creating build/scripts-2.7
copying bin/rpirtscts -> build/scripts-2.7
creating build/bdist.linux-armv7l/egg/EGG-INFO/scripts
copying build/scripts-2.7/rpirtscts -> build/bdist.linux-armv7l/egg/EGG-INFO/scripts
changing mode of build/bdist.linux-armv7l/egg/EGG-INFO/scripts/rpirtscts to 755
copying ublox_lara_r2.egg-info/PKG-INFO -> build/bdist.linux-armv7l/egg/EGG-INFO
copying ublox_lara_r2.egg-info/SOURCES.txt -> build/bdist.linux-armv7l/egg/EGG-INFO
copying ublox_lara_r2.egg-info/dependency_links.txt -> build/bdist.linux-armv7l/egg/EGG-INFO
copying ublox_lara_r2.egg-info/requires.txt -> build/bdist.linux-armv7l/egg/EGG-INFO
copying ublox_lara_r2.egg-info/top_level.txt -> build/bdist.linux-armv7l/egg/EGG-INFO
zip_safe flag not set; analyzing archive contents…
creating dist
creating ‘dist/ublox_lara_r2-0.0.1-py2.7.egg’ and adding ‘build/bdist.linux-armv7l/egg’ to it
removing ‘build/bdist.linux-armv7l/egg’ (and everything under it)
Processing ublox_lara_r2-0.0.1-py2.7.egg
Copying ublox_lara_r2-0.0.1-py2.7.egg to /usr/local/lib/python2.7/dist-packages
Adding ublox-lara-r2 0.0.1 to easy-install.pth file
Installing rpirtscts script to /usr/local/bin
Installed /usr/local/lib/python2.7/dist-packages/ublox_lara_r2-0.0.1-py2.7.egg
Processing dependencies for ublox-lara-r2==0.0.1
Searching for pyserial==3.2.1
Best match: pyserial 3.2.1
Adding pyserial 3.2.1 to easy-install.pth file
Using /usr/lib/python2.7/dist-packages
Finished processing dependencies for ublox-lara-r2==0.0.1
pi@raspberrypi:~/ublox_lara_r2_pi_hat $ cd test
pi@raspberrypi:~/ublox_lara_r2_pi_hat/test $ sudo python test01.py
assuming 40-pin GPIO header
Enabling CTS0 and RTS0 on GPIOs 16 and 17
rts cts on
waking up… …
module name: LARA-R211
RSSI: 99
pi@raspberrypi:~/ublox_lara_r2_pi_hat/test $
Bill