LTE Cat 1 Pi HAT - Further steps and APN

Hi,



I have used the LTE Cat 1 Pi HAT shield for US carriers both AT&T and VERIZON using the Hologram sim. This hologram sim otherwise connects to Verizon or AT&T signal based on the available network. I have following questions:


  1. Will I require to configure APN ? If yes which file or AT commands can I use for that purpose?


  2. I followed the steps given here: [/http://wiki.seeedstudio.com/LTE_Cat_1_Pi_HAT/], I did get all the output as expected, with RSSI 7. But I still cannot to the internet, is there another script to keep it connected to the internet? Will I get a static IP after connection? Basically what is to be done next?



    Best,

    Vishwas

Hi Vishwas



We are writing the APN examples and will update the wiki later on. thanks.

I have the same issue, I see that 2 years have passed without any updates?

Any updates yet??? Its sad to buy something with a lot of promise – only to find out that its JUNK because it has zero support! I’m getting really sick of this.