HI ,
I Want to build a low energy vibration detection system using XIAO nRF52840 (Sense).
I wanted some advise on how to ensure that the device can run for at least a few months on 3000 mAh battery .
I want the device to send data either every 5 seconds in case there is an vibration event or send nothing to save power .
The application is going to use the 6 Axis accelerometer to detect the vibration and use the ML model to classify the vibration in one of the 7 states . In case there is a valid event it should be transmitted else it sleeps .
I do not know how to write a low energy application like this , kindly suggest a path which I can follow.