LoRapedia, an Introduction of LoRa and LoRaWAN Technology

What are LoRa and LoRaWAN? What are the differences between them and how they contribute to the IoT industry? Here we write a tech blog about Semtech LoRa to help both users and practitioners of the industrial IoT to understand LoRa & LoRaWAN in a broader sense by knowing about the technological structure, features, and applications of LoRa & LoRaWAN!

To read the article, click the link here: https://www.seeedstudio.com/blog/2020/08/03/lorapedia-an-introduction-of-lora-and-lorawan-technology/

2 Likes

@ellen010726 Where is the average user most likely to use LoRa technology?

1 Like

Hi there,

So I’m resurrecting this thread… It’s topic is one that is in need of Review and Refresh
I like this thing…

Pretty sweet. ! :+1:

HTH
GL :slight_smile: PJ :v:

1 Like

I wish i could get someone from seeed to help with this… because as you can see,.. i cant type right… and in case anyone is wondering… I have been having problems with my eyesight, which causes me to bring my face closer to the screen and that messes up my hand placement over the keyboard and splays my hands out and so my muscle memory is wrong… someone accused me of typing while drunk… and while that also may be a thing sometimes… it is hot the drinking that causes the bad typing… it causes the bad additude… lol joking… kinda