Looking for place to upload Wio Terminal .ino file & information.
Will be of interest for people wanting to do their own password & file security.
Nothing complex please.
Thank You!
Bob
Looking for place to upload Wio Terminal .ino file & information.
Will be of interest for people wanting to do their own password & file security.
Nothing complex please.
Thank You!
Bob
Scrambler Wio
Scrambler Wio is small device that is used to keep, and to send and receive private information. It consists of an open source program “Scrambler2(29 Aug 23A).ino” running in a Wio Terminal with a SD card. Reference “https://wiki.seeedstudio.com/Wio-Terminal-Getting-Started/”.
Scrambler Wio’s main function is to scramble and unscramble files using four dedicated subdirectories on the SD card; “ScrambleIn”, “ScrambleOut”, “UnScrambleIn” and “UnScrambleOut”. Files in ScrambleIn are scrambled and placed in ScrambleOut with a file extension of “.SCB”. The files in ScrambleIn are overwritten and deleted in this process. “*.SCB” files in UnScrambleIn are unscrambled and placed in UnScrambleOut. The files in UnScrambleIn are deleted in this process.
The “*.SCB” files contain the original file information in randomized bytes that randomly appear in a file of random bytes that is over four times larger than the original file. The scrambling/unscrambling is controlled by a 4 to 10 digit “KEY” and static data in the program and in the SD card. All three of these are required for the successful scrambling and unscrambling of files! Only somebody with the exact three will be able to unscramble files created by these three. The static data in the program and the SD card are intended to be independently set up for a particular user or set of users.
The Scrambler program will take the user through four modes in the following order.
The 2nd and 4th modes use a mini-editor and is only intentioned to be used for simple editing. It displays/uses special “symbols” for new-line (carriage-return) and blank as follows: ‘Ç’ & ‘
︎’. The display only displays the basic english characters. All other characters (bytes) are replaced with blank. It is intended to edit/view things like passwords/pins that will only leave Scrambler Wio by it’s display or in scrambled files.
The mini-editor input is by the Wio joystick. It is used to move through a file’s characters or to select a different character. A joystick-press is alternately used to select a file character or a different character. A different character is selected by navigating a 4 line by 26 character table of available characters (see following table). This table also includes 2 special characters, ‘«’ & ‘»’ for backspace and insert. To save the file and/or exit press the edge button opposite the joystick.
The “different character” table:
« » Ç
︎ 0 1 2 3 4 5 6 7 8 9 . , “ ‘ - ? : ! ;
a b c d e f g h i j k l m n o p q r s t u v w x y z
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
& _ ` ~ @ # $ % ( ) = + - * / ^ < > { } \ |
The 3rd mode is controlled by a simple display/interface.
The joystick is used to control the entry of digits into the displayed “KEY”, and to select actions as follows:
‘<‘ will remove the last entered digit.
‘>’ will use the displayed “KEY” to scramble and unscramble files.
‘R’ will reset this 3rd mode to it’s original state.
‘M’ will use the displayed “KEY” to mutate the program.
‘E’ will exit without scrambling and unscrambling files.
‘?’ is a spare action (and is the same as ‘E’).
Scrambler Wio can not guaranty that files stay private. Only a knowledgeable user can do that.
Notes:
Know Bugs or Issues:
Hi,Good research,We have published a contrbutor wanted program, you can change the wiki contents, accept some assignments or share your thoughts with us. We will offer a range of rewards to our contributors.