I want to use one of the on board SATA power connectors to power a M.2 NGFF NVMe Key M to PCIe 3.0 X16 Extension Cable. I am not adding a GPU, but rather a SuperMicro dual port SFP+ card. The converter has a plug to get power. It is 4 pin, 12v.
I would like to buy a cable to connect the two.
Here is the M.2 NGFF NVMe Key M to PCIe 3.0 X16 Extension Cable;
https://www.amazon.com/gp/product/B08CB679C5/
It almost looks like a FAN connector on that one. But it is hard to say. I won’t have that part for a week or so.
Any help is greatly appreciated.
Brian