I would call this a success!
All it needed was this line in .conf:
CONFIG_FLASH=y
Thanks everyone here for the friendly help, I hope this will someday help someone else to not spend days for this ![]()
I’m currently trying to run the nRF54L15 with Zephyr. For future reference, I’d really appreciate your help with the following:
Thank you for the information.
The link below shows the current data from an experiment where 8 bytes were transferred every 10 seconds. For your reference!
Hi @raffiniert
Can you tell me if you explicitly suspended the flash in your code like below?
// Put the peripheral into suspended state.
int err = pm_device_action_run(qspi_dev, PM_DEVICE_ACTION_SUSPEND);
In the older versions of nrf connect I had to suspend the flash with ported arduino code. In my last go the above code was used. Maybe a recent update removes the need for explicit suspend of the flash. If so, I’ll update my example code. I’ll also double check that it doesn’t brick the xiao.
Payback time for all the help I got on this forum!
I try to document my cleanup of everything I’ve tried.
Removing this function in main() costs me 8uA:
static void qspi_flash_enter_dpd_and_park_pins(void)
{
/* Init QSPI long enough to talk to the chip */
nrfx_qspi_config_t cfg = NRFX_QSPI_DEFAULT_CONFIG(19, 17, 20, 21, 22, 23);
cfg.pins.sck_pin = 19;
cfg.pins.csn_pin = 17;
cfg.pins.io0_pin = 20;
cfg.pins.io1_pin = 21;
cfg.pins.io2_pin = 22;
cfg.pins.io3_pin = 23;nrfx_qspi_init(&cfg, NULL, NULL); /* Send Enter Deep Power-Down (0xB9) */ nrf_qspi_cinstr_conf_t cin = { .opcode = 0xB9, .length = NRF_QSPI_CINSTR_LEN_1B, .io2_level= true, .io3_level= true, .wipwait = false, .wren = false, }; (void)nrfx_qspi_cinstr_xfer(&cin, NULL, NULL); /* Done with QSPI */ nrfx_qspi_uninit(); /* Park pins to prevent leakage: CS high, others pulled down */ const struct device *gpio0 = DEVICE_DT_GET(DT_NODELABEL(gpio0)); gpio_pin_configure(gpio0, 17, GPIO_OUTPUT_HIGH); /* CS */ gpio_pin_configure(gpio0, 19, GPIO_INPUT | GPIO_PULL_DOWN); /* SCK */ gpio_pin_configure(gpio0, 20, GPIO_INPUT | GPIO_PULL_DOWN); /* IO0 */ gpio_pin_configure(gpio0, 21, GPIO_INPUT | GPIO_PULL_DOWN); /* IO1 */ gpio_pin_configure(gpio0, 22, GPIO_INPUT | GPIO_PULL_DOWN); /* IO2 */ gpio_pin_configure(gpio0, 23, GPIO_INPUT | GPIO_PULL_DOWN); /* IO3 */}
WIP