When starting up I have to pull the sender (tx/rx) out of the usb port and plug it back in for the mouse and keyboard to work.
This is the same on two different boards. ( I bought 3)
The same in all USB ports
The same with two different models of Mouse/Keyboard combos
What’s the problem? How can I fix it?
Running the Windows Enterprise that came with the board… all updated and activated.
Deleted and reinstalled driver