Lipo Rider Pro: Programming Mode

Is there anything to do, to be able to program an arduino connected to the LiPo Rider Pro Board ?

quote seeedstudio.com/wiki/Lipo_Rider_Pro
In case solar power is not sufficient, the microUSB port allows you to charge your lithium battery through USB. It can also be used to program your kit without detaching the LiPo Rider Pro board.

If I connect my PC, using the MINI-USB INPUT Port on the LiPo Rider Pro Board and the Arduino using the USB OUTPUT Port, my PC does not recognize the arduino as USB Device ( same with android handy )

( the switch is on of course :slight_smile: )

hi~ cu’z the u+ and u- line of usb port of lipo-rider has not been connected~ so, maybe you can weld the two line up by a wire~ :smiley: