LinkStar-H68K-0232 Router Firmware Updates

I am very impressed with the specifications of the LinkStar-H68K, however, it’s a bit disappointing to read that it supports Ubuntu, then purchase the device, wait for it to arrive, then learn [1] the allegedly available versions of Ubuntu (for this device) don’t yet support WiFi (which is the main selling feature of the device), and [2] there are actually NO versions of Ubuntu available to download for this device, and no indication as to what to realistically expect. Very disappointing!

3 Likes