Hi,
I am in the process of developing a low cost tracking device.
I am planning following steps:
- Purchase LinkIt ONE
- Using following link, create GPS tracker prototype
<LINK_TEXT text=“http://www.instructables.com/id/LinkIt- … dbox-tuto/”>http://www.instructables.com/id/LinkIt-ONE-GPS-Tracker-MediaTek-Cloud-Sandbox-tuto/</LINK_TEXT>
(or)
- Using MediaTek LinkIt SDK create GPS tracker prototype
- On successful testing make production units with MT2502 and MT3332.
I have doubt on step 4. If I look at the “LinkIt ONE”, the GPRS, GSM & Bluetooth sections are under shield as one unit.
But I need only MT2502 and MT3332 and other necessary components for mass production.
How can I achieve this?, as I worked with “LinkIt ONE”, as a complete kit, and not as individual sections?