Light / Deep Sleep Current Comparison of XIAO_MG24 and XIAO_nRF52840

There is an example of an external pin wake-up on the Examples, which worked well.
It is hard to find the wake-up requirements in the datasheet because there are multiple low power levels.

1 Like