Licence Code FFFFFFFF

Hi, I need a licence Code for DSO Quad HW 2.8.1 (Device Firmware V3.45C)

Serial Number is 79339F9D - Many thanks if anyone can still help

Hello, I can’t seem to pinpoint your product well based on this. Can you send me the full product name or sku if it’s convenient? I can try to look it up for you.

Thanks for answering. To be honest I am not sure, I lent it to a colleague and finally got it back… He has changed the installed FW… At the start up screen (after like 20 attempts at reading before realising MObile videos would be good):
FPGA Configuration OK!
Hardware Ver 2.81 Serial No: 79339F9D
DS203 Mini DSO SYS Ver 1.64

In OS: SAme INfo + DFU Version: V3.45C

DSO_APP(1): Gabonator’s Alternative UI
Firmware Version: rev. 134535289

Hi there,
Check this thread…

HTH
GL :slight_smile: PJ

“modified” means, he skipped the license verification.

you mean this? :smiley:

I want to put the default Image back, I found all the data to do it (I think) and now I just want to get the correct Licence NUmber so everything is ready to flash at the weekend

(post deleted by author)