Library conflicts nRF52840 Sense

Hi there,
Great to hear that, There is a learning curve but it’s not Too heavy a lift though.
Here are some ways to stop BLE on an nRF52840:

  • Start and stop advertising: Use sd_ble_gap_adv_start() and sd_ble_gap_adv_stop()
  • Disconnect from the central: Use sd_ble_gap_disconnect() while in a connection
  • Stop scanning with BLE.end(): While the peripheral is off, stop scanning with BLE.end()
  • Disable completely the 2.4Ghz radio: After the 52840 has full soft device enabled and ble stack has been run, disable completely the 2.4Ghz radio

HTH
GL :slight_smile: PJ