Library conflicts nRF52840 Sense

Hello PJ.

Yes, the example blink_print in the timer library is interesting. But I do not understand the toggle principle.
My timer needs pulse of 1 to 2 ms. Then, in the LOW time, the duration of the next pulse is calculated.
Then, after 8 ms since the beginning of the first pulse, everything happens again.
Could you lease look at that sketch, and give me an indication for the solution?
Kind regards,

Wolfgang
P.S Started 50 years ago with FORTRAN. :slight_smile: