Li-po Rider

Hi everyone,

I would like to know which version is the Li-po Rider module in the Seeedstudio Store: http://www.seeedstudio.com/depot/lipo-rider-p-710.html?cPath=155
Is this the V0.9b or V1.2? (http://garden.seeedstudio.com/index.php?title=Lipo_Rider)
And which are the practical differences between them in terms of specifications and performance?

Finally, which are the main practical differences between the Li-po Rider and the Solar Charger shield (http://www.seeedstudio.com/depot/solar-charger-shield-p-594.html?cPath=155) when both used with Arduino/Seeeduino boards powered by 2000mAh or 3300mAh (http://www.seeedstudio.com/depot/lithium-ion-polymer-batteries-2a-p-603.html or http://www.seeedstudio.com/depot/lithium-ion-polymer-batteries-3300mah-p-605.html?cPath=178_183) battery and a 1w solar panel for charging (http://www.seeedstudio.com/depot/1w-solar-panel-75x100-p-633.html?cPath=155)?

Thanks!
João Rodrigues

Hello,
We are sorry for confusing.
It is the Lipo Rider v1.0, the v1.2 is the document version.
Thanks
Albert

Hi,

Thanks for your answer!

The board’s documentations really led me to believe that there were two versions of the board: 0.9 and 1.2 (garden.seeedstudio.com/index.php … Lipo_Rider).

Just to clarify my other doubt, is this module suitable for my propose? Which are the practical differences and similarities with the Solar Charger shield?

João Rodrigues