I checked that there is a python version (pixel_ring) of controling the LEDs on ReSpeaker Core V2.
Now testing some source localization algorithms, I wonder how to do it using C/C++.
Could anyone provide an example? Or maybe I should explore something like USB-HID.
Thanks in advance
Hello,
I would like to use Respeaker 4mic Led with C++ language, I can’t find any example with this language.
Is it possible to get some example?
Regards,
For the respeaker pi hat led, please refer to <URL url="https://forum7.seeedstudio.com/t/control-leds-using-c-and-spi-respeaker-4-mic-array/6713/1]<LINK_TEXT text=“viewtopic.php?f=87&t=32048”>https://forum7.seeedstudio.com/t/control-leds-using-c-and-spi-respeaker-4-mic-array/6713/1]
we do not have the respeaker core v2.0 led c++ code yet.
thanks.