- Arduino IDE: v1.8.16
- Board Package: Seeed XIAO RP2040 v1.9.3
I referred to the XIAO RP2040 Wiki and tried to get the Examples > 01.Basics > Blink working.
But, I get the following error when compiling.
Wiki: https://wiki.seeedstudio.com/XIAO-RP2040-with-Arduino/
"C:\\Users\\user\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\tools\\pqt-gcc\\1.3.1-a-7855b0c/bin/arm-none-eabi-g++" -c -Werror=return-type "-IC:\\Users\\user\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\hardware\\rp2040\\1.9.3/tools/libpico" -DCFG_TUSB_MCU=OPT_MCU_RP2040 -DUSB_VID=0x2e8a -DUSB_PID=0x000a "-DUSB_MANUFACTURER=\"Raspberry Pi\"" "-DUSB_PRODUCT=\"Pico\"" -Os -march=armv6-m -mcpu=cortex-m0plus -mthumb -ffunction-sections -fdata-sections -fno-exceptions "-iprefixC:\\Users\\user\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\hardware\\rp2040\\1.9.3/" "@C:\\Users\\user\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\hardware\\rp2040\\1.9.3/lib/platform_inc.txt" -fno-rtti -std=gnu++17 -g -DSERIALUSB_PID=0x000a -DF_CPU=125000000L -DARDUINO=10816 -DARDUINO_RASPBERRY_PI_PICO "-DBOARD_NAME=\"RASPBERRY_PI_PICO\"" -DARDUINO_ARCH_RP2040 "-IC:\\Users\\user\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\hardware\\rp2040\\1.9.3\\cores\\rp2040" "-IC:\\Users\\user\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\hardware\\rp2040\\1.9.3\\variants\\rpipico" "C:\\Users\\user\\AppData\\Local\\Temp\\arduino_build_426700\\sketch\\XIAORP2040_Blink.ino.cpp" -o "C:\\Users\\user\\AppData\\Local\\Temp\\arduino_build_426700\\sketch\\XIAORP2040_Blink.ino.cpp.o"
C:\Users\user\Documents\Arduino\XIAORP2040_Blink\XIAORP2040_Blink.ino: In function 'void setup()':
XIAORP2040_Blink:32:11: error: 'LED_BUILTIN' was not declared in this scope
32 | pinMode(LED_BUILTIN, OUTPUT);
| ^~~~~~~~~~~
C:\Users\user\Documents\Arduino\XIAORP2040_Blink\XIAORP2040_Blink.ino: In function 'void loop()':
XIAORP2040_Blink:37:16: error: 'LED_BUILTIN' was not declared in this scope
37 | digitalWrite(LED_BUILTIN, HIGH); // turn the LED on (HIGH is the voltage level)
| ^~~~~~~~~~~
exit status 1
'LED_BUILTIN' was not declared in this scope
Looking at variants/rpipico/pins_arduino.h on the board package, it seems that LED_BUILTIN is not defined.
#define LED_BUILTIN PIN_LED