iura
1
Hi
I setup arduino uno with Base shield v2
temp sensor works, heart rate sensor works etc
but LCD doesn’t show text
even with “hello world” example
i can change colour of display with
const int colorR = 255;
const int colorG = 0;
const int colorB = 0;
but
lcd.print("hello, world!");
doesn’t work
loovee
2
Hi, is there a connection image of you project, thanks.
tahuff
3
I have a similar problem with with the Grove shield on an Arduino Duemilanove. Here is my setup and the sketch I’m using:
#include <Wire.h>
#include “rgb_lcd.h”
rgb_lcd lcd;
const int colorR = 255;
const int colorG = 0;
const int colorB = 0;
void setup()
{
// set up the LCD’s number of columns and rows:
lcd.begin(16, 2);
void setRGB(int colorR, int colorG, int colorB);
// Print a message to the LCD.
lcd.print("hello, world!");
delay(1000);
}
Any help would be appreciated. Could it be a faulty display?
kavi
4
Hello,
When using with duemilanove solder the pads P1 and P2(shown in the attachment) in the grove base shield v2.
Let us know if it works.
Thanks and Regards