LCD EXT breakout board question

Hi, I have a question about the 0.5mm LCD ext breakout board:

seeedstudio.com/depot/lcd-ex … p-200.html

I have an 8 pin FFC with 0.5 pitch that I need to breakout. However a different breakout board I ordered wouldn’t hold the FFC because it was too thin. The FFC is about 0.3 mm thick. Will this breakout board accommodate this thickness of FFC?

Yes, it is 0.3mm thick FFC compatible.