Hello,
I have a new BeagleBone Green Gateway and I’m following the instructions here: https://wiki.seeedstudio.com/BeagleBone-Green-Gateway/
Step 2 is install drivers. For mac they give links for both ‘Network’ and ‘Serial’ drivers. Attempting to install either on my mac running macOS Big Sur 11.5.2 results in:
“This package is incompatible with this version of macOS.”
I’m wondering if the serial one is even needed anymore because I do see a usb device show up as the following when it’s plugged in:
/dev/cu.usbmodem2020060003825
Regardless, all of the subsequent steps rely on connecting to it over ethernet which I’m assuming is accomplished via the network driver install.
Are there updated mac network drivers to install that are compatible with the instructions?