Hi guys,
I’ve the L298 Dual H-Bridge Motor Driver ( seeedstudio.com/depot/l298-d … th=170_173 ) and a spare unipolar stepper motor with 6 wires ( KH56KM2-016 ), is possible to use it with the unipolar motor? All should be drived by a seeduino…
Hi guys,
I’ve the L298 Dual H-Bridge Motor Driver ( seeedstudio.com/depot/l298-d … th=170_173 ) and a spare unipolar stepper motor with 6 wires ( KH56KM2-016 ), is possible to use it with the unipolar motor? All should be drived by a seeduino…
Up, how is possible that anyone have never used that driver with a stepper motor? 
As far as I know, L298 can only drive a four wire two phase step-motor.
Yes but the motor is driven as a bipolar ( with the half coil disconnected ), is a common solution to use with 6 wires unipolar motor and should work. 
I’ve loaded on the seeduino the tutorial sketch founded here: arduino.cc/en/Tutorial/StepperBipolar but all I get is just a sort of motor vibration.
I’m sure I’m doing something wrong with the connections, the documentation for the l298 driver is not very clear: for example the documentation say only “EA is connecting with PWM port of control board to control the speed of motor” but is only for DC motor or I still need to provide a pwm signal also for the stepper?
Yes, EA and EB need to be connected to +5V/set to HIGH.