Join Error, when using SenseCAP M2 Gateway with OTAA on AWS IoT Core for LoRaWAN

Hello.
I tried to use several LoRaWAN sensor devices via SenseCAP M2 Gateway on AWS IoT Core for LoRaWAN.
but, when OTAA activation settings, it occured join error continuously.

In addition, I checked the followings.

  • when ABP activation settings on AWS IoT Core for LoRaWAN, it operated normaly.
  • when OTAA activation settings on TTN, it operated normaly.
  • when OTAA activation settings using other gateway(dragino LPS8N) on AWS IoT Core for LoRaWAN, it operated normaly.

environment:

  • Frequency Plan: AS923-1
  • Device: seeed Tracker T1000-A, seeed Wio-E5 mini, dragino LT-22222-L, dragino LA66-USB
  • Gateway: seeed SenseCAP M2 gateway, dragino LPS8N

Has anyone encountered the same problem and resolved it?

Does anyone have any information?

Access the SenseCAP M2’s log files to see if the OTAA join requests from devices are being received and forwarded to AWS IoT Core. Look for:

Errors indicating dropped packets or rejected requests.
Mismatches in DevEUI, AppEUI, or AppKey.

Hi, I’ve tried to reproduce your issue in our test environment but didn’t find the problem as you described, both devices (seeed Sensor S2103, seeed Tracker T-1000A) are successfully connected to AWS IoT Core with OTAA activation settings.

Below is the environment of M2 Gateway:

  • Build Version: r1-20220615
  • OS Version: 0.9.3-4
  • Firmware Version: 1.2.0-25
  • LoRaWAN Region: AS923
  • LoRaWAN Network Mode: Basics Station
  • Server: LNS Server

I refer to this Wiki for the process of configuring gateways and devices Connecting to AWS IoT.

Sorry for the late reply.
Thank you for the useful reference information.

Currently, M2 Gateway works fine on AWS IoT.
The cause may be the automatic update of basic station on M2 Gateway.

  • Basic station version and build date and time at the time of error
    Station Ver: 2.0.6(corecell/std) 2022-10-13 13:08:29

  • Normal basic station version and build date and time
    Station Ver: 2.0.6(corecell/std) 2024-11-05 06:28:32

  • Other version information
    Model: M2-AS923
    Build Version: r1-20220615
    OS Version: 0.9.4-5
    Firmware Version: 1.2.0-25
    LoRaWAN Region: AS923