I have a jetson mate and I need to press the wake button to power up
is there any to auto power up?
Hi, have you found a solution for this yet?
For our needs it’s imperative that our Jetson board plugging into the Jetson Mate auto power up when connected to a power source yet it appears one must press the “wake” button on the Jetson Mate for the Jetson board to actually boot. I’m not seeing anything about this in the wiki here. I’d be most appreciative if anyone has any thoughts on this.
I’m interested in this as well. Has anyone found a solution?
I came across this if you’re comfortable doing a little surface mount soldering: JETSON TX2 AUTO-POWER-ON - Jetson TX2 - NVIDIA Developer Forums
…Unfortunately, that is the only option I’ve found 
+1 absolutely needed. is there a place to make feature requests.
+1 here too. any news?