Jetson DevelopTool installation

I’m trying to install Jetson DevelopTool on Ubuntu 24.04 and it fails with messages about missing libgl1-mesa-glx. It won’t let me separately install libgl1-mesa-glx because it says it was ‘transitional’ and has been replaced.

Hi there,

So, You’re running into a classic dependency breakage on Ubuntu 24.04 because the tool (or an older script/dependency it relies on) is trying to pull in libgl1-mesa-glx, which was deprecated and completely removed from Ubuntu repositories starting with version 23.10 and newer.

To fix it without hacking up the system package manager too much, they need to update the tool package or handle the missing OpenGL libraries cleanly.

The standard fix options for that error on Ubuntu 24.04 include:

  • Update to the latest package release: If they installed via pip, they should pull the latest patch where these legacy transitional dependencies have been cleaned up:
python3 -m pip install --upgrade seeed-jetson-developer

nstall modern Mesa alternatives: If an older script insists on the library, Ubuntu 24.04 maps those functions to libgl1 and libglx-mesa0 instead.
or
Run via container/distrobox: Running the installer inside an isolated container image (like Ubuntu 22.04 LTS) avoids host-level library mismatches entirely when dealing with older NVIDIA flashing and development tools.

There is a Set of terminal commands , you can use to fix it also, longer but does the same thing.
creates a dummy package type of thing.
they other is Map to Modern Native Equivalents (Best for scripts and python environments)

If you are modifying a script, a requirements.txt, or a custom shell installer, replace references to libgl1-mesa-glx with modern equivalents that supply the exact same OpenGL rendering functions on Ubuntu 24.04:

sudo apt update
sudo apt install libgl1 libglx-mesa0 libgl1-mesa-dev

Verification: Run apt-cache policy libgl1 libglx-mesa0 to confirm both packages are active and mapped to your system architecture.

HTH

GL :slight_smile: PJ :v:

Thanks! The Map to Modern Native Equivalents for libgl1, and adding a few more missing things like ssl one by one eventually worked.

Seeed, if you see this, a Seeed Jetson DevelopTool install procedure that includes all the required packages and just works on new Ubuntu Desktops would be really helpful for overworked teachers.

1 Like