Jetpack 6.0 on reComputer Industrial-series

I can see that the J401 carrier board has a guide on how to flash with JP 6.0, here. What are the plans on JP 6 support on the reComputer Industrial-series? Or are there anyone who have successfully flashed such device with JP 6?

I have a reComputer Industrial ‘J4011’ which I can flash with JP 6 using the NVIDIA SDK Manager. However, after flashing I have access to only one of the two network interfaces. The other one is UNCLAIMED when looking at lshw. My guess is that there is a driver missing.

Thanks in advance!

We expect to release it by the end of June. Stay tuned!

2 Likes

Hi again! Are there any progress on this?