Java.io.IOException & Error Downloading

To resolve this issue:

  1. Update to Installation Manager version 1.4.2.

  2. Open the config.ini file located in the Installation Manager installation location. By default, this location is:

Windows: C:\Program Files\IBM\Installation Manager\eclipse\configuration\config.ini
Linux and UNIX: /opt/IBM/InstallationManager/eclipse/config.ini

  1. Remove the following two properties:

cic.retry.move
cic.skip.FileDescriptor.sync

Note: If the error is received during an Installation Manager update from 1.4.1 to 1.4.2, disable file monitoring software and retry the update.

Regards,
Peter