J4012 Jetpack 6 No wifi

Dear community,

I am currently experiencing significant difficulties with my Seeed ReComputer Orin NX 16GB setup and seek your assistance.

Problem Description:

  1. Wi-Fi Module:
    Hardware: Intel 8265NGW.
    Jetpack: 6 (Installed as guided on the Seeed’s procedure)
    Issue: Although the Wi-Fi module is connected, the system indicates “No Wi-Fi adapter found.” Only the Ethernet connection is functional.
    Troubleshooting Steps Taken:
    Attempted installation of drivers using sudo apt install iwlwifi-modules. This approach did not resolve the issue, although it worked previously when I flashed the Seeed NX with the SDK Manager.
    Downloaded the driver from Intel’s website, copied it to /lib/firmware, reinstalled linux-firmware, and rebooted. This also did not resolve the issue.
  2. USB to CAN Connection:
    The connection is not being established, despite following standard procedures.

Additional Context:

The same ubuntu setup especially concernned with the CAN setup has been tested and works flawlessly on other devices, including Jetson Orin Nano, NUCs, and AGX.
The issues seem to be isolated to the Seeed ReComputer Orin NX 16GB and Seeed ReComputer Orin Nano 4GB.

I am seeking guidance on resolving these issues promptly, as it is critical for my ongoing projects. Your assistance and recommendations would be greatly appreciated.

Thank you for your support.