On J4012 (Orin NX 16GB) I’ve put jetpack 6 as instructed in WIKI.
Previously on Jetpack 5.1.1, the Intel AX200i. Now on JP6, the Wi-fi doesn’t work. Only LAN connection works ![]()
On J4012 (Orin NX 16GB) I’ve put jetpack 6 as instructed in WIKI.
Previously on Jetpack 5.1.1, the Intel AX200i. Now on JP6, the Wi-fi doesn’t work. Only LAN connection works ![]()
We will be coming out with a new version of the JP6 image pack in the near future. We apologize for any inconvenience caused!
HI there!
On wiki I see this version:
mfi_recomputer-orin-nx-16g-j401-6.0-36.3.0-2024-07-04.tar.gz
Is the new one? I do not remember the exact version I flashed a week ago.
Thank you!
I’ll flash it today! ![]()
The flash image it seems to be bugger than the last one.
There are less errors, but I still cannot make the Intel AX200 to work properly…
I have to test some more workarounds
[I still cannot make the Intel AX200 to work properly…]
I am experiencing a similar issue. I am looking for a solution.
Dear community,
I am currently experiencing significant difficulties with my Seeed ReComputer Orin NX 16GB setup and seek your assistance.
Problem Description:
sudo apt install iwlwifi-modules. This approach did not resolve the issue, although it worked previously when I flashed the Seeed NX with the SDK Manager./lib/firmware, reinstalled linux-firmware, and rebooted. This also did not resolve the issue.Additional Context:
The same ubuntu setup especially concernned with the CAN setup has been tested and works flawlessly on other devices, including Jetson Orin Nano, NUCs, and AGX.
The issues seem to be isolated to the Seeed ReComputer Orin NX 16GB and Seeed ReComputer Orin Nano 4GB.
I am seeking guidance on resolving these issues promptly, as it is critical for my ongoing projects. Your assistance and recommendations would be greatly appreciated.
Thank you for your support.
We apologize for the inconvenience! We will review the image package we provided again. Troubleshooting to see if this problem occurs
@shashank CAN is for driver motor control?
Our engineers have only done testing for Intel 8265NGW at this time. If there is a situation where the WiFi module is not recognized, you can follow the steps below:
sudo rm /lib/modules/5.15.136-tegra/build
sudo ln -s /usr/src/linux-headers-5.15.136-tegra-ubuntu22.04_aarch64/3rdparty/canonical/linux-jammy/kernel-source/ /lib/modules/5.15. 136-tegra/build
sudo apt install -y iwlwifi-modules
reboot
Hope the above steps will help you!
Thank you @Seeed_Seraphina! After your response I’ve tried several times exactly how it was written and after many errors I’ve made it work. On your second line of terminal commands I think there’s a
typo error
/lib/modules/5.15. 136-tegra/build
Here I think is an extra SPACE character after 5.15.
This is what has worked in my case. Perhaps there are unnecessary commands and some linux guru can make it better.
sudo rm /lib/modules/5.15.136-tegra/build
sudo ln -s /usr/src/linux-headers-5.15.136-tegra-ubuntu22.04_aarch64/3rdparty/canonical/linux-jammy/kernel-source/ /lib/modules/5.15.136-tegra/build
sudo apt install -y iwlwifi-modules
sudo apt update
sudo apt upgrade
sudo reboot
sudo modprobe iwlwifi
sudo lspci | grep Network
sudo dmesg | grep iwl
nmcli device wifi list
Yes! CAN is for the VESC I am using. I use the 4 wheel drive robot and hence I need CAN so that I can drive it on the differential wheel drive.
I will try the solution @Seeed_Seraphina @Vivio you have given for the WiFi and get back to you soon!
Thanks
In my case the drivers are two Odrive’s. I have to see if I’ll use an Raspberry PI with CAN hat as slave and Orin NX as master or NX can drive directly the CAN hat.
In your cas is an USB 2 CAN solution, right?
Hello to all, I own a Jetson Orin Nano 8GB
I was able to flash the JetPack version 6.x following the Docs: Flash Jetpack | Seeed Studio Wiki
I have now a blocking problem, because I’m not able to restore the WiFi connection: I get always the error Unable to locate package iwlwifi-modules
Here my output: unnamed hosted at ImgBB — ImgBB
I hope @Seeed_Seraphina can help me, because I really don’t know what is happening
Hello @lunard .
I would like to confirm two points of information to you:
Hello community, Nvidia recently released Jetpack 6.2 with Super Power Mode. I have tried to use SDK Manager and CLI options to flash the J4012 with the new Jetpack 6.2, but they are both unable to identify the board.
I am a beginner to this field so I do not fully understand why is there a difference between Nvidia Dev Board and carrier dev board in terms of updating the new software?
I am using J4012 Jetson Orin Nx board btw.
Hi there,
And Welcome here,
SO first they are not the same, SO refer to the WiKi for your unit J4012, look at the matrix and see if it’s supported or released yet.
ALso the method to upgrade or reflash is different and doesn’t support the Nvidia SDK manager update.
Read up on the JP6.1 threads also.
HTH
GL
PJ ![]()
Please open a new thread suggesting your issue, we are still testing the jetpack 6.2 and will release our jetpack 6.2. SDK Manager was mainly for official devkits only, which doesn’t contain certain BSP information we have.
That worked for me after flashing to JetPack 6.2. Thank you! My module is AC8265, J4012 board.
It worked fine on JetPack 5 but failed after upgrade.