Here is the version details of my DSO -
Hardware Ver V2.70
DS203 Mini DSO SYS Ver 1.52
DS203 Mini DSO APP (PLUS A1) Ver 1.00
I’ve already faced some confusion regarding this DSO. It would be great if the user answer my following queries -
Is it the latest one?
I can set 10v maximum in ChA and ChB. So, is it the maximum voltage that can be seen using 1X probe? If yes, using 10x probe I can view only 100v. Right?
Can I connect 10x probe directly to our power line (230v AC)? If I want to view voltage waveform greater then the maximum rating of this what will happen? Will it be damaged? or it will show some error message?