🐉 It is TIME for a New Dragon... this is the year "XIAO nRF5340 " Dragon

:dragon_face: :dragon_face:
Time for a two headed new Dragon , Seeed can make a drop in upgrade in Speed and Power efficiency just by swapping chips and minimal changes. WIN/WIN for everyone and seeed again leads the way in Innovation… Besides this year is the year of the Dragon. Let’s go !!!

They could do us a solid and drop in the range extender chip(nRF21540 - nordicsemi.com) and really blow Stuff up!

Between 6.3-10x range extension when combined with an nRF52 or nRF53 Series SoC
C’mon man that’s a no brainer :brain:

They have a superior PMIC as well , dump the crap :poop: battery charge ic. on the Xiao BLE & Sense.
time for an Upgrade…

Xiao 5340 Dragon.

no more RPi for me thanks… :face_vomiting:

Very funny… LOL :smiley: :grinning: :smile: :grin:
Who sent me two SEEED Xiao RP2350’s and two GPIO expanders.
looks like jello, and I always have room for jello… :yum:

trying to send me a message… LOL I’ll look them over.
here is sort of all that matters imo. But ZERO connectivity or serial only Deal breaker because a radio is a basic fundamental item in todays internet of things connected world. IMO.

Features

  • Powerful MCU Board: Equipped with a Raspberry Pi RP2350 chip featuring symmetric dual Arm Cortex-M33 @ 150MHz with FPU.
  • Enhanced Security Features: Built-in secure boot and encrypted bootloader ensure application security.
  • Software Support: Compatible with C/C++ and MicroPython, ensuring easy project development and prototyping.
  • Rich Onboard Resources: Integrates an RGB LED, 2MB Flash, 520kB SRAM, and 19 multifunction GPIOs(Analog, Digital, I²C, UART, SPI, PWM).
  • Expanded 8 New IOs: Compared to previous XIAO MCUs, the addition of 8 IO pins on the back supports more complex applications.
  • Efficient Power Design: Ultra-low power consumption of just 27μA in sleep mode, enabling battery power supply. Direct battery voltage measurement via internal IO enhances the battery management system (BMS).

HTH
GL :slight_smile: PJ
:v:

Santa Seeed please send me this…nRF5340 plug in and upgrade in a Xiao form factor add the PMIC and WIFI scanner chip. :muscle: TAKE over market. :dragon: :rocket:
BAM


:v:

nRF7002+nRF5340 WiFi 6+BLE 5.3 Combo Module MS12SF1 2.4G and 5G Two Wireless Connection Mode Module
WOW, someone beat you too it…

proves it can still be small like Xiao. :heart_eyes: :+1:

DHL.
Working OT in my area.
Just got the latest in Development and prototype hardware bases from Nordic local rep as promised. Its a bargain for the DualCore nRF5340 development platform and the JLink alone. The thingy is more of a prototyping platform and contains many sensors. I’ll be introducing them and demonstrating some of the possibilities. With the next generation of Fresh hardware.
Coded PHY here we go!



Same size, consistent design.

Stay tuned.
GL :slight_smile: PJ :v:

1. Processing Power & Architecture:

  • nRF5340:

    • Dual-Core Design: It features a 128 MHz Arm Cortex-M33 application processor and a 64 MHz Cortex-M33 network processor. This separation of application and network tasks can lead to more efficient processing and lower latency, particularly in complex applications.
    • Dedicated Network Processor: The network core is optimized for handling radio protocols like Bluetooth LE, ensuring that the application core is free for other tasks.
  • ESP32S3/C6:

    • ESP32S3: It has a single-core Xtensa LX7 processor, capable of running at up to 240 MHz. The dual-core architecture (found in the ESP32) is absent in the S3, which could lead to more contention between application and communication tasks.
    • ESP32C6: Features a RISC-V single-core processor and adds support for Wi-Fi 6, but again, lacks a dedicated core for networking tasks.
1 Like

The future is here…

New Dragon with real FIRE!

nRF5340 SoC

Dual-core Bluetooth 5.4 SoC supporting Bluetooth Low Energy, Bluetooth mesh, NFC, Thread and Zigbee

128 MHz Arm Cortex-M33 CPU with
1 MB Flash + 512 KB RAM
64 MHz Arm Cortex-M33 CPU with
256 KB Flash + 64 KB RAM
Bluetooth Low Energy
Bluetooth Direction Finding
Bluetooth mesh
Thread, Zigbee
ANT
NFC
Advanced security
USB, QSPI, HS-SPI
105 °C extended operating temperature
1.7-5.5 V supply voltage range


Angle of arrival and angle of departure
Bluetooth Direction Finding is based around the two key concepts of angle of arrival (AoA) and angle of departure (AoD). This makes use of the angular phase-shifts that occur between antennas as they receive (AoA) or transmit (AoD) RF signals.

With the use of antenna arrays at either side of the communication link phase shift data can be determined and from this, location can be calculated.

Seriously… :face_with_peeking_eye: :vulcan_salute:

Bluetooth Direction Finding is the major feature of the Bluetooth 5.1 Core specification. It is designed to enhance location services where previously only signal strength based technology has been used with received signal strength indication (RSSI).

Bluetooth Direction Finding will offer new and improved use case for real time location systems (RTLS) for asset tracking in a wide range of scenarios from logistics and warehousing to value asset security in hospitals and factories. It also brings added user experiences in proximity-based scenarios for consumer awareness and contextual information.

Bluetooth Direction Finding can be used to detect location in either 2D or 3D dependent on the complexity of its implementation.

C’mon smart guys… Break some new ground !

GL :slight_smile: PJ :v:

2 Likes

Hi, PJ!

Can’t find this info anywhere in the Internet, but do you know what nrf5340 chip is doing in the nrf52840 DK?

Hi there,

Why, Yes indeed…:grin: I saw that a while back and
the Clue was when I recieved the Nrf54L15 DK :grin:

further investigation leads to this from AL…
Both the nRF52840-DK and the nRF54L15-DK use a dedicated nRF5340 SoC as the onboard debugger/programmer.

Details:

  • Part Number on Debugger Chip: Usually marked something like nRF5340-QKxx or similar.

  • It runs Nordic’s Segger J-Link OB (OnBoard) firmware.

  • Handles:

    • SWD/SWO programming/debugging
    • UART bridge (Virtual COM port)
    • Drag-and-drop .hex programming (via MSD)
    • Sometimes also USB DFU support
  • Acts as a bridge between USB (host PC) and the actual target MCU (nRF52840 or nRF54L15)

  • Nordic switched to the nRF5340 as the debugger chip because it has:

  • Dual-core (App + Net)

  • Better USB support

  • Lower power standby while remaining USB-connected

  • It replaces older chips like the nRF52820 or nRF52832 used in previous DKs

HTH
GL :slight_smile: PJ :v:

1 Like

now it makes perfect sense! Thanks!

Funny, I look for information about the “new” nRF7002 wifi companion chip and What do I find? a PJ post from last year. Which leads me to ask, Why isn’t there one of these available yet?
Looks like it’s pretty much a drop-in wifi addon for the nordic low power chips.
(Technical Documentation)

1 Like

Hi there,

Yep, It’s a true dual core as well, and all the debuggers use them.?
I have the NRF7002 add-on brd, nice hardware forsure. :+1:
This nRF54 Series is supposed to be the future, so jury is still out on this seat. :grin:

HTH
GL :slight_smile: PJ :v:

Yeah, I’m designing an add-on for the Xiao 54 in my head it has one of these, and either qspi flash or a tf card slot.

1 Like