This is to inform that we are using a carrier board version A203 (V2) and we have attached the SOM module with it and with the help of SDK manager we flashed the OS and got the installation done right.
But on inserting the SD card it is giving the issues and not able to detect the card
On referring to the document we found that there are some drivers which are required to be installed i.e. inside the kernel we need to replace the dtb file.
But this also doesn’t resolve the issue. It detects the SD card at once but after reboot SD card is shown in the device list and also we are not able to mount it and format it again.
We are aware of this issue and will update the documentation as soon as possible so that the installation of the driver can be completed successfully. We expect to complete this within the next week.
Waiting for the driver update…we want it ASAP…please provide support for this…if you have any other method to mount SD card then please let us know that also
sudo ./flash.sh ${BOARD} mmcblk0p1
My suggestion is to replace the files and reinstall the system using the above command. Also note in particular that the driver is only supported by JetPack 4.6
You need to be careful to download the corresponding driver package according to the module you are using, the driver packages for nano and nx are not the same.