Hi,
I am facing the issue with the Grove Vision AI camera module. I do not know if there is a possibility to combine the Trained model with Arduino code.
Actually, I followed some tutorials on Seeed wiki which focuses on trained models and deploying that model to the device by coping the files of the trained model to the drive Grove AI
What I want is the code of Arduino or some standalone C++ code which runs on the Grove Vision module and sends some of the detection results via interface such as Grove etc.
So do you know is it yet possible with Grove Vision AI module or some third party software can help in this case??
In fact, we are in talks to support Edge Impulse and are pleased that Edge Impulse will complete support for Vision AI as soon as possible, so when that happens, the output of the results from the models will be done through Arduino programming, so stay tuned.
Hi, as this product is currently designed, to recognise other models you may need to train them yourself or download them from some model websites (of course, we will go on to do this piece specifically in the future). Vision AI can then output the number of models identified to your model and its confidence level. The output is all done in C/C++.
For more information, please refer to the Wiki below.
I’ve seen something similar. I flash the Face Detection model via USB and Senscraft page. Then unplug the USB and plug it into an Arduino (via I2C) and the model is gone.
That does sound like the model isn’t actually being committed to flash, or the board is booting into a different firmware/state when powered from the Arduino side.
A couple of things worth checking: after uploading in SenseCraft, safely disconnect/reboot the module and reconnect it to the PC first to confirm the model is still there before moving to Arduino. Also make sure the Arduino is supplying stable power; weak 3.3V/5V rails can cause odd boot behavior. If the model disappears consistently after power cycling, please share the exact Grove Vision AI module version and the SenseCraft/flashing steps you used — that would help narrow down whether this is a firmware issue or a flashing workflow issue.
Also worth Noting is the BSP you use on the Arduino side and the Schema LIB. check your versions and dates.
That being said, it does work.
Keep at it, You’ll get it working, You are close.