Issue with Respeaker 4-Mic and Pimoroni/Pirate Audio AMP Shim

I think I know that answer, but look for confirmation and possible alternatives from much smarter people.

I’m looking to use Respeaker 4-Mic and Pimoroni Audio AMP shim for a Mycroft build.

I believe this is a conflict between the two hats. Depending on the order of the overlays in the /boot/config.txt, the last hat in the config works.

[all]
dtparam=i2s=on
dtoverlay=i2s-mmap
hdmi_enable_4kp60=1
#enable_tvout=1
gpio=25=op,dh
dtoverlay=seeed-4mic-voicecard
dtoverlay=hifiberry-dac

I’m dead set on using the ReSpeaker 4-mic, so if there is a conflict between the 2, what are my options?

I don’t want to use the onboard audio. Is it possible to deconflict the two devices or does anyone have a recommendation for a audio hat similar to Pimoroni Audio Amp Shim?