Hello,
I designed my first shield for usage with an arduino. On the shield three ports are available to connect the 7 Segment and the LCD from Grove with the Arduino I2C. I have no Issue operating the Segment or the LCD alone but as soon as I connect both of them the LCD starts displaying weird signs after a while and the code stops. From the past I know the code is not the issue. There is something wrong with the design of the layout e.g. I am missing Pullup resistors on SCL and SDA which I attached currently extern onto the shield!
I have attached some pictures of the board design. Is there anything I have to take additionally in account regarding the LCD?
According Segment: https://www.adafruit.com/product/1270