Issue with e-ink display contrast fading after refresh - GxEPD2, XiaoESP32-S3 with ePaper, GDEY075T7

I’m working with a 7.5" e-Paper display (GDEY075T7) connected to a XIAO ESP32 S3 using the GxEPD2 library. After refreshing the display, I’m experiencing contrast fade-out where the previously clear black image gradually lose clarity.

My code, with the help of Claude 3.7, downloads BMP images via WiFi and displays them on the e-ink screen. I use GxEPD2 Library to program the display. The text and drawing function works properly as intended.

Current implementation includes:

  • GxEPD2_BW library with GDEY075T7 panel
  • WiFi downloading of bitmap images
  • Standard refresh cycle with display.refresh()
  • Anti-ghosting attempt with clearScreen()

I’m trying various ways to debug the code, but I’d love to know if anyone here:

  1. Has experience loading BMP images over Wi-Fi to an e-ink display and getting them to render properly without fadeout
  2. Can help determine whether this is a hardware or software issue that’s causing the display to behave this way.

Thank you so much!

Below is a sequence of screenshots showing what happens when the image loads:

  • The image briefly appears with proper contrast (less than a second)
  • It immediately enters a refresh sequence
  • Then the image fades out, with a horizontal line appearing across it

Hi there,

And Welcome here…

So The e_ink can be finicky But the Boards BSP can also play a part, Which BSP did you use to compile it with? Can you post your Code using the code tags above “</>” just paste it in there. Lots of smart folks on here can comment.

Looks like weather map data pictures?

HTH
GL :slight_smile: PJ :v: