Is it possible to get gyro values from LIS3DHTR IMU in Wio Terminal?

By definition, in IMU sensor, it is possible to measure gyro signals like pitch rate, roll rate, and yaw rate.

However I cannot find the examples which can measure the gyro signals.
Also in the LIS3DHTR.h.

It is not possible? or there must be an update in library?

@ansonhe97 Please add gyro to the examples

Hi @youngil_sohn

LIS3DHTR is a 3 axis accelerometer but not a gyro.

@youngil_sohn You can find the LIS3DHTR examples here: Seeed-Studio/ Seeed_Arduino_LIS3DHTR .

ok. understood. Hope to get IMU sensor included Wio terminal in near future.

Hi @youngil_sohn

I have used Wio terminal to make a little gyro ball demo before. You can read this for some reference.

#include <TFT_eSPI.h>                 // Include the graphics library (this includes the sprite functions)

TFT_eSPI    tft = TFT_eSPI();         // Create object "tft"
TFT_eSprite img = TFT_eSprite(&tft);  // Create Sprite object "img" with pointer to "tft" object
// the pointer is used by pushSprite() to push it onto the TFT

#include"LIS3DHTR.h"
LIS3DHTR<TwoWire> lis;

#define SPEED 5 //Higher the quicker
#define COLOR TFT_RED //Color of circle
#define SIZE 18 //Size of Circle

float x_raw, y_raw, z_raw;
float roll, pitch, rollF, pitchF=0;

void setup(void) {
    tft.init();
    tft.setRotation(0);
    
    Serial.begin(115200);
    lis.begin(Wire1);
  
    if (!lis) {
      Serial.println("ERROR");
      while(1);
    }
    
    lis.setOutputDataRate(LIS3DHTR_DATARATE_25HZ); //Data output rate
    lis.setFullScaleRange(LIS3DHTR_RANGE_2G); //Scale range set to 2g   

}

void loop() {
    img.createSprite(TFT_WIDTH, TFT_HEIGHT);
    img.fillSprite(TFT_BLACK);
 
    x_raw = lis.getAccelerationX();
    y_raw = lis.getAccelerationY();
    z_raw = lis.getAccelerationZ();

//    Serial.print(x_raw);
//    Serial.print(" ");
//    Serial.print(x_raw);
//    Serial.print(" ");
//    Serial.println(z_raw);

    roll = atan(y_raw / sqrt(pow(x_raw, 2) + pow(z_raw, 2))) * 180 / PI;
    pitch = atan(-1 * x_raw / sqrt(pow(y_raw, 2) + pow(z_raw, 2))) * 180 / PI;
    
    // Low-pass filter
    rollF = 0.90 * rollF + 0.10 * roll;
    pitchF = 0.90 * pitchF + 0.10 * pitch;
    
    Serial.print(rollF);
    Serial.print("/");
    Serial.println(pitchF);

    // BOTTTOM BOUNDARY
    if (TFT_WIDTH/2+(-pitchF)*SPEED >= TFT_WIDTH-SIZE) {
      if (TFT_HEIGHT/2+(rollF)*SPEED >= TFT_HEIGHT-SIZE) { // LEFT CORNER
        img.fillCircle(TFT_WIDTH-SIZE, TFT_HEIGHT-SIZE, SIZE, COLOR);
        img.drawCircle(TFT_WIDTH-SIZE, TFT_HEIGHT-SIZE, SIZE+0.5, TFT_WHITE);
      }
      else if (TFT_HEIGHT/2+(rollF)*SPEED <= SIZE) { // RIGHT CORNER
        img.fillCircle(TFT_WIDTH-SIZE, SIZE, SIZE, COLOR); 
        img.drawCircle(TFT_WIDTH-SIZE, SIZE, SIZE+0.5, TFT_WHITE);
      }
      else {
        img.fillCircle(TFT_WIDTH-SIZE, TFT_HEIGHT/2+(rollF)*SPEED, SIZE, COLOR);
        img.drawCircle(TFT_WIDTH-SIZE, TFT_HEIGHT/2+(rollF)*SPEED, SIZE+0.5, TFT_WHITE);
      }
    }

    // TOP BOUNDARY
    else if (TFT_WIDTH/2+(-pitchF)*SPEED <= SIZE) {
      if (TFT_HEIGHT/2+(rollF)*SPEED >= TFT_HEIGHT-SIZE) { // LEFT CORNER
        img.fillCircle(SIZE, TFT_HEIGHT-SIZE, SIZE, COLOR);
        img.drawCircle(SIZE, TFT_HEIGHT-SIZE, SIZE+0.5, TFT_WHITE);
      }
      else if (TFT_HEIGHT/2+(rollF)*SPEED <= SIZE){ // RIGHT CORNER
        img.fillCircle(SIZE, SIZE, SIZE, COLOR);
        img.drawCircle(SIZE, SIZE, SIZE+0.5, TFT_WHITE);
      }
      else {
      img.fillCircle(SIZE, TFT_HEIGHT/2+(rollF)*SPEED, SIZE, COLOR);
      img.drawCircle(SIZE, TFT_HEIGHT/2+(rollF)*SPEED, SIZE+0.5, TFT_WHITE);
      }
    }

    // LEFT BOUNDARY
    else if (TFT_HEIGHT/2+(rollF)*SPEED >= TFT_HEIGHT-SIZE) {
     img.fillCircle(TFT_WIDTH/2+(-pitchF)*SPEED, TFT_HEIGHT-SIZE, SIZE, COLOR);
     img.drawCircle(TFT_WIDTH/2+(-pitchF)*SPEED, TFT_HEIGHT-SIZE, SIZE+0.5, TFT_WHITE);
    }
    // RIGHT BOUNDARY
    else if (TFT_HEIGHT/2+(rollF)*SPEED <= SIZE) {
     img.fillCircle(TFT_WIDTH/2+(-pitchF)*SPEED, SIZE, SIZE, COLOR);
     img.drawCircle(TFT_WIDTH/2+(-pitchF)*SPEED, SIZE, SIZE+0.5, TFT_WHITE);
    }
    //DEFAULT
    else {
      img.fillCircle(TFT_WIDTH/2+(-pitchF)*SPEED, TFT_HEIGHT/2+(rollF)*SPEED, SIZE, COLOR);
      img.drawCircle(TFT_WIDTH/2+(-pitchF)*SPEED, TFT_HEIGHT/2+(rollF)*SPEED, SIZE+0.5, TFT_WHITE);
    }

    img.pushSprite(0, 0);
    img.deleteSprite();

}

You can work out roll and pitch using accelerator readings.

thanks. however this is not measuring method , but estimation from 3axis accelerometer.
Anyway, I found the way to accomplish my task.

in the next version of this Wio terminal, I hope to see real IMU with real gyro sensors.