Hi,
i plan to buy a DSO 203 (quad).
And I would like to know if it is possible to solder a microSD slot on the Mainboard of the DSO 203 and mod the firmware so that it will work like in a DSO 202?
Daniel
Hi,
i plan to buy a DSO 203 (quad).
And I would like to know if it is possible to solder a microSD slot on the Mainboard of the DSO 203 and mod the firmware so that it will work like in a DSO 202?
Daniel
I’d see if you can find an image of the board. My guess is that it’s pretty tight inside the unit.
I’m kind of surprised they didn’t include a microSD slot, even if the functionality wasn’t programmed in right away.
the DSO Quad has a USB disk(2M) for firmware upgrading and saving the waveform. it is more convenient than sd card i think although a bit small.