I want to do a board that is oddly shaped, the outline and dimensions are in the image below
Would the board be cut to this shape or should I design as a simple rectangle and to the cutouts myself when I receive the boards? Anyone have experience ordering board shapes like this?
Just keep in mind that the radius of the inner corners will be limited by the router bit they use (typically 2mm or so diameter). Normally, this doesn’t matter; if it is critical you could clean up the corners with a file by hand.